s32k312 example code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k312 example code

6,407件の閲覧回数
coo
Contributor I

Hello.

I installed S32DS for S32 and Extensions.

I use s32ds 3.5 ver

When I choose "New --> S32DS Project form Example" menu, there is only for S32K358, 344.

Is there way to get S32K312 example project?

Thank you.

0 件の賞賛
返信
8 返答(返信)

6,023件の閲覧回数
chenhua
Contributor II

跟着大佬们一起学习NXP

0 件の賞賛
返信

6,027件の閲覧回数
chenhua
Contributor II

看你们牛弹琴,我也学会了。

0 件の賞賛
返信

6,380件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport
 
Sorry for the inconvenience we bring you!
Seems that you are using S32K3 RTD 3.0.0 or higher.
It did not offer S32K312 examples when you choose "New --> S32DS Project form Example" menu.
You need to create S32K312 project by refer to S32K344.
or
Refer to S32K312 examples in S32K3 RTD 2.0.0 + S32DS v3.4.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,312件の閲覧回数
coo
Contributor I
I'm trying to download s32ds version 3.4 and use S32K3 RTD 2.0.0.
But there is only S32K3 RTD AUTOSAR 4.4 version 2.0.0 in s32ds extensions and updates, is this right?
0 件の賞賛
返信

6,309件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I have installed S32K3 RTD 2.0.0 - 2.0.3 offline for S32DS v3.4. I am not sure whether S32K3 RTD 2.0.3 will be displayed in your S32DS Extensions and Updates. If not, please offline install S32K3 Real-Time Drivers Version 2.0.3.

0 件の賞賛
返信

6,051件の閲覧回数
John64
Contributor I
Hi Robin, 

 How to install the S32K312 example in S32DS v3.5?

In S32DS V3.5 Extensions and Updates the S32K3 RTD 3.0.0, and it included S32K344/358 example code not S32K312. 

6,028件の閲覧回数
chenhua
Contributor II

原来如此,怪不得呢。thanks 

0 件の賞賛
返信

6,042件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes. S32K3 RTD 3.0.0 and 4.0.0 did not offer S32K312 examples. You may need to create it by yourself. Fortunately FAE provides some examples here for RTD 3.0.0 S32K312: All Example S32K312 DS3.5 RTD-3.0.0