internal clock deviation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

internal clock deviation

ソリューションへジャンプ
1,677件の閲覧回数
yangaichimantou
Contributor I

Hi,

We need S32K to calculate high precision time.

We want to know, if we use external crystal of 16M and frequency tolerance of 1 ppm.

S32K internal clock double 10x frequency by PLL.

Then the internal time deviation may be 10 times of the external crystal deviation?

Or do we have other experiment data or calculate method?

0 件の賞賛
返信
1 解決策
1,663件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@yangaichimantou

yes ,you can calculate it like this, but it's not entirely accurate.

because the PLL has a filtering effect on the input source jitter, there is inherent PLL jitter on the generated output,so a completely accurate calculation is not easy to quantify.

BR!

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,664件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@yangaichimantou

yes ,you can calculate it like this, but it's not entirely accurate.

because the PLL has a filtering effect on the input source jitter, there is inherent PLL jitter on the generated output,so a completely accurate calculation is not easy to quantify.

BR!

 

 

0 件の賞賛
返信