how to use the EB Tresos generates the code--(EB Tresos Studio 27.1.0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to use the EB Tresos generates the code--(EB Tresos Studio 27.1.0)

跳至解决方案
5,761 次查看
Guofred
Contributor III

Open EBTresos and click File -> Import -> General -> Existing Projects 
into Workspace
, select the template project McAl_template_project_dio_47811a_440_100. zip installation Path into which the Tresos project is imported.  when i click the somld , some error comes out .the details as below. 

Guofred_3-1639652849687.png

Guofred_4-1639652952145.png

Guofred_5-1639653007689.png

What causes this problem and how can I fix it, thanks.

Best regards.

Guofred

 

 

 

0 项奖励
回复
1 解答
5,743 次查看
namnguyenviet
NXP Employee
NXP Employee

The problem is EB Tresos couldn't find the MCAL package. You need to install the MCAL package which correspond to the project you're using, by copy to the EB/tresos/plugins folder.

Best Regards,

Nam

在原帖中查看解决方案

0 项奖励
回复
2 回复数
5,744 次查看
namnguyenviet
NXP Employee
NXP Employee

The problem is EB Tresos couldn't find the MCAL package. You need to install the MCAL package which correspond to the project you're using, by copy to the EB/tresos/plugins folder.

Best Regards,

Nam

0 项奖励
回复
5,739 次查看
Guofred
Contributor III

Hi @namnguyenviet ,

Ok, thanks for your help.

Best regards.

Guofred 

0 项奖励
回复