error about burn the program into board when use different debuggers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error about burn the program into board when use different debuggers

1,972 Views
Xjh193
Contributor III

Hello!

Fault Occurrence Scenario:

different debuggers were used alternately to burn the program without powerdown. debuggers are PE debugger and trace32 debugger. 

Fault description :

1 PE cannot connect to target board.

2 trace32 display error "running locked up".

Looking forward to your help.

 

0 Kudos
Reply
3 Replies

1,962 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Xjh193,

You did not specify the MCU.

Are there any details about the errors provided by the debuggers?

 

BR, Daniel

0 Kudos
Reply

1,944 Views
Xjh193
Contributor III

hello @Daniel.

I used S32K344 MCU. I used trace32 to burn program into board when the board is powered on for the first time. Debugger display "bus error at address APB:0x8000AFE0".

There is another question is that why I deleted many source to compile project,trace32 “list source” function is ok. If not to delete, the function can't work. When I add a huge array into the project deleted many source. The function“list source”  is also not ok. Can you tell me why?

Looking forward to you help!

0 Kudos
Reply

1,931 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Xjh193,

What program/examples are you trying to flash?

Can you use the latest RTD RTM 2.0.0 examples from S32DS 3.4?

 

BR, Daniel

0 Kudos
Reply