XRDC secure and non secure access policy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XRDC secure and non secure access policy

Jump to solution
1,937 Views
UmaMaheswaraReddy
Contributor IV

What is Secure Access policy and non secure access policy? What is the difference between them?

I didnt find any info regarding this S32K3 RM and RM UM.

 

UmaMaheswaraReddy_0-1709829748255.png

 

0 Kudos
Reply
1 Solution
1,899 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @UmaMaheswaraReddy 

Summarizing, the PIDs are used to create multiple classes of cores, each in different domains. please refer to sections 19.5.5.2 (PID-based domain assignment) and 19.5.7.2 (DFMT0 PID-based domain assignment example) of the S32K3 reference manual. 

Additionally, the S32G family has an XRDC module. This family has an application note that explains in more detail this module. I recommend you to use it as a reference. 

IMPORTANT: The modules ARE SIMILAR, but they are NOT THE SAME, so you need to take care and consider the differences between the technologies. 

AN13024: S32G2 Extended Resource Domain Controller (XRDC) Application Note

View solution in original post

0 Kudos
Reply
3 Replies
1,913 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @UmaMaheswaraReddy 

These define the access depending on the permissions. I am afraid that the S32K3 real-time drivers do not use the same terminology as the S32K3 reference manual, causing confusion and problems in finding the information.

Please refer to sections 19.5.6.7.1 (Access control model levels), 19.5.6.7.2 (Generation of secure attribute), and 19.5.6.8 (Domain ACP specification) of the S32K3xx Reference Manual, Rev. 8, for more information.

 

B.R.

VaneB

0 Kudos
Reply
1,902 Views
UmaMaheswaraReddy
Contributor IV

Thank you for the info. 

I am also confused with the PID. Understood that PIDS are used for domain assignment and it is optional. I checked S32K3XX RM (XRDC) but I am unable to get clear info on this.

We have direct domain assignment. Why PID based domain assignment? In what/which cases we choose PID based domain assignment?

 

 

0 Kudos
Reply
1,900 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @UmaMaheswaraReddy 

Summarizing, the PIDs are used to create multiple classes of cores, each in different domains. please refer to sections 19.5.5.2 (PID-based domain assignment) and 19.5.7.2 (DFMT0 PID-based domain assignment example) of the S32K3 reference manual. 

Additionally, the S32G family has an XRDC module. This family has an application note that explains in more detail this module. I recommend you to use it as a reference. 

IMPORTANT: The modules ARE SIMILAR, but they are NOT THE SAME, so you need to take care and consider the differences between the technologies. 

AN13024: S32G2 Extended Resource Domain Controller (XRDC) Application Note

0 Kudos
Reply