Why is the red box part missing from my software,os part and middleware part
解決済! 解決策の投稿を見る。
Hi @SCoder41
Check if you can find it in the "Previous" tab.
元の投稿で解決策を見る
Just to confirm, did you install the FreeRTOS and TCPIP packages compatible with your RTD version?
B.R.
VaneB
What do I need to do
To install this TCPIP package, you require the FreeRTOS package version 1.0.0 release for S32K3 platforms, which supports FreeRTOS Kernel v10.4.5. This can be downloaded through S32K3 Reference Software -> Automotive SW - S32K3 - FreeRTOS.
I do not see 10.4.5 in S32K3 Reference Software -> Automotive SW - S32K3 - FreeRTOS.
I had installed,but I'm not sure if the version I installed is correct or not