Why must open the ‘EcuM WakeUP source’ parameter when configuration the Lin moudle in MCAL EB tresos

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why must open the ‘EcuM WakeUP source’ parameter when configuration the Lin moudle in MCAL EB tresos

1,775 次查看
ananan
Contributor III

As shown below, when I do not configure the EcuM WakeUP Source, an error is reported at compile time in the red box below

ananan_0-1636005421975.png

But when I add the EcuM module (add the WakeUP source) and it turns on the EcuM WakeUP Source, the error disappears

ananan_1-1636005734480.png

I don't want to use Ecum module, and I don't want to turn on LIN wake up function, how should I configure, I don't know what to do

0 项奖励
回复
1 回复

1,762 次查看
hungnguyenphi
NXP Employee
NXP Employee

Hello @ananan ,

 

This is a limitation in the MCAL_4.3_RTM_1.0.1. Could you please try the newest version MCAL_4.3_RTM_1.0.2.

 

Best regards,

Hung.

0 项奖励
回复