Why must open the ‘EcuM WakeUP source’ parameter when configuration the Lin moudle in MCAL EB tresos

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why must open the ‘EcuM WakeUP source’ parameter when configuration the Lin moudle in MCAL EB tresos

2,335 Views
ananan
Contributor III

As shown below, when I do not configure the EcuM WakeUP Source, an error is reported at compile time in the red box below

ananan_0-1636005421975.pngananan_0-1636005421975.png

But when I add the EcuM module (add the WakeUP source) and it turns on the EcuM WakeUP Source, the error disappears

ananan_1-1636005734480.pngananan_1-1636005734480.png

I don't want to use Ecum module, and I don't want to turn on LIN wake up function, how should I configure, I don't know what to do

0 Kudos
Reply
1 Reply

2,322 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @ananan ,

 

This is a limitation in the MCAL_4.3_RTM_1.0.1. Could you please try the newest version MCAL_4.3_RTM_1.0.2.

 

Best regards,

Hung.

0 Kudos
Reply