Unable to Install NXP GCC for ARM Embedded Processors v10.2 (Build 1728) in S32 Design Studio v3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to Install NXP GCC for ARM Embedded Processors v10.2 (Build 1728) in S32 Design Studio v3.4

1,522 Views
vk_669
Contributor I

I am facing an issue while installing required packages in S32 Design Studio v3.4. The installation is failing because the default package NXP GCC for ARM Embedded Processors v10.2 (Build 1728) cannot be installed. Though it is written it is an optional package but still it is being downloaded once I click on install on any required package. This is preventing the setup of other necessary components.

Has anyone encountered this issue? Any guidance on resolving this would be greatly appreciated.

Thanks!

 

This is the issueThis is the issue

0 Kudos
Reply
1 Reply

1,497 Views
RomanVR
NXP Employee
NXP Employee

Hi @vk_669.

Similar situations have been discussed in the community before. Please take a look at the following community thread and let me know if the solution provided there was helpful to you. 

error in installing extension.

- RomanVR.

Best Regards!
0 Kudos
Reply