Unable to Install NXP GCC for ARM Embedded Processors v10.2 (Build 1728) in S32 Design Studio v3.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to Install NXP GCC for ARM Embedded Processors v10.2 (Build 1728) in S32 Design Studio v3.4

1,634件の閲覧回数
vk_669
Contributor I

I am facing an issue while installing required packages in S32 Design Studio v3.4. The installation is failing because the default package NXP GCC for ARM Embedded Processors v10.2 (Build 1728) cannot be installed. Though it is written it is an optional package but still it is being downloaded once I click on install on any required package. This is preventing the setup of other necessary components.

Has anyone encountered this issue? Any guidance on resolving this would be greatly appreciated.

Thanks!

 

This is the issueThis is the issue

0 件の賞賛
返信
1 返信

1,609件の閲覧回数
RomanVR
NXP Employee
NXP Employee

Hi @vk_669.

Similar situations have been discussed in the community before. Please take a look at the following community thread and let me know if the solution provided there was helpful to you. 

error in installing extension.

- RomanVR.

Best Regards!
0 件の賞賛
返信