Trying to run example code lwip_s32k344 but getting errors during compilation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trying to run example code lwip_s32k344 but getting errors during compilation

1,646件の閲覧回数
Ajesh
Contributor I

Trying to run example code lwip_s32k344 but getting errors during compilation Invalid project path: Include path not found (\SW32K3_RTD_4_4_2_0_0_D2203\Base_TS_T40D34M20I0R0\header). I am using DS3.5

 

Ajesh_0-1697104912187.pngAjesh_0-1697104912187.png

 

0 件の賞賛
返信
3 返答(返信)

1,594件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Ajesh , 

 

Please can you check if include file path doesn't contain additional " " or it can be caused by missing RTD/SDK installation or wrong user configuration.

 

For this go to: 

Right click on project -> project properties → C/C++ Build → Settings → Standard S32DS C Compiler → Includes.

 

Please can you share the screenshot of the current properties to check. 

 

Thank you. Best regards. 

-Mehul Patel

0 件の賞賛
返信

1,608件の閲覧回数
Ajesh
Contributor I

Ajesh_0-1697692136958.pngAjesh_0-1697692136958.png

Please find above

I am using DS3.4 along with SW32_S32DS_3.4.0_D2012

SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204

but compilation is failing.

Ajesh_1-1697692286219.pngAjesh_1-1697692286219.png

 

0 件の賞賛
返信

1,617件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share full build console output? What is the error message? You shown only warnings. 

0 件の賞賛
返信