Trying to run example code lwip_s32k344 but getting errors during compilation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trying to run example code lwip_s32k344 but getting errors during compilation

1,660 Views
Ajesh
Contributor I

Trying to run example code lwip_s32k344 but getting errors during compilation Invalid project path: Include path not found (\SW32K3_RTD_4_4_2_0_0_D2203\Base_TS_T40D34M20I0R0\header). I am using DS3.5

 

Ajesh_0-1697104912187.png

 

0 Kudos
Reply
3 Replies

1,608 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Ajesh , 

 

Please can you check if include file path doesn't contain additional " " or it can be caused by missing RTD/SDK installation or wrong user configuration.

 

For this go to: 

Right click on project -> project properties → C/C++ Build → Settings → Standard S32DS C Compiler → Includes.

 

Please can you share the screenshot of the current properties to check. 

 

Thank you. Best regards. 

-Mehul Patel

0 Kudos
Reply

1,622 Views
Ajesh
Contributor I

Ajesh_0-1697692136958.png

Please find above

I am using DS3.4 along with SW32_S32DS_3.4.0_D2012

SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204

but compilation is failing.

Ajesh_1-1697692286219.png

 

0 Kudos
Reply

1,631 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share full build console output? What is the error message? You shown only warnings. 

0 Kudos
Reply