Software funcional reset and FCCU functional duration (FS26 enabled)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software funcional reset and FCCU functional duration (FS26 enabled)

ソリューションへジャンプ
1,720件の閲覧回数
FabioG
Contributor III

Hi there, 

On some tests seem that  after a software reset (2ms of duration on RESET_b pin) the consecutive reboot happens 92 ms later (all GPIO in 3-state and no software running).

Executing a fault injection on a FCCU channel configured as "short reset", this time grows to more than 250 ms and FS26 triggers an unwanted destructive reset.

Why FCCU soft reset is so long?

where I Find these s32k reboot times, i don't find them in DS or RM.

Best Regards,

Fabio

 

 

 

0 件の賞賛
返信
1 解決策
1,705件の閲覧回数
FabioG
Contributor III

Problem resolved !

Thank you

Fabio

元の投稿で解決策を見る

3 返答(返信)
1,256件の閲覧回数
JRodrigues
Contributor III

Hello @FabioG,

 

How did you solve this issue? I'm having the same problem!

 

Best Regards,

JRodrigues

0 件の賞賛
返信
1,706件の閲覧回数
FabioG
Contributor III

Problem resolved !

Thank you

Fabio

1,623件の閲覧回数
Yetkin
Contributor I
Hi FabioG,

How did you solve it? I am facing the same problem.

0 件の賞賛
返信