Software funcional reset and FCCU functional duration (FS26 enabled)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software funcional reset and FCCU functional duration (FS26 enabled)

Jump to solution
1,695 Views
FabioG
Contributor III

Hi there, 

On some tests seem that  after a software reset (2ms of duration on RESET_b pin) the consecutive reboot happens 92 ms later (all GPIO in 3-state and no software running).

Executing a fault injection on a FCCU channel configured as "short reset", this time grows to more than 250 ms and FS26 triggers an unwanted destructive reset.

Why FCCU soft reset is so long?

where I Find these s32k reboot times, i don't find them in DS or RM.

Best Regards,

Fabio

 

 

 

0 Kudos
Reply
1 Solution
1,680 Views
FabioG
Contributor III

Problem resolved !

Thank you

Fabio

View solution in original post

3 Replies
1,231 Views
JRodrigues
Contributor III

Hello @FabioG,

 

How did you solve this issue? I'm having the same problem!

 

Best Regards,

JRodrigues

0 Kudos
Reply
1,681 Views
FabioG
Contributor III

Problem resolved !

Thank you

Fabio

1,598 Views
Yetkin
Contributor I
Hi FabioG,

How did you solve it? I am facing the same problem.

0 Kudos
Reply