Smoke detector interfacing with FS32K146HAT0MLLT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Smoke detector interfacing with FS32K146HAT0MLLT

Jump to solution
2,703 Views
ultra12
Contributor III

I am using MQ-2 smoke detector in my design.The sensor is working at 5V supply.This sensor has both analog and digital outputs.

I am using analog output in my design.The microcontroller used is FS32K146HAT0MLLT from NXP.The controller is also working at 5V.

The analog output varies from 0V to 5V so I did not use any voltage scaling circuit between sensor and microcontroller.

A LPF of cut off frequency 1.6Khz(arbitrarily chosen) is kept at the output of sensor.

May I know this circuit is fine or do I need to take care any other things.

 
ultra12_4-1702459871223.pngultra12_4-1702459871223.png

 

 

 

In the datasheet I can see a current limit resistor(RL).Is that necessary. How do I design that resistor.

 
ultra12_2-1702459823710.pngultra12_2-1702459823710.png

 

 
Tags (1)
0 Kudos
Reply
1 Solution
2,677 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I would attach such guide for selecting components external to ADC. Although written for different device, used SAR ADC is very similar module, they may be minor differences in specified values.

Hope it helps

View solution in original post

1 Reply
2,678 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I would attach such guide for selecting components external to ADC. Although written for different device, used SAR ADC is very similar module, they may be minor differences in specified values.

Hope it helps