Sequence Error with FTM-PDB-ADC Triggering

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sequence Error with FTM-PDB-ADC Triggering

跳至解决方案
12,394 次查看
bjrajendra
Senior Contributor I

Hello all,

I'm using S32K146 device and I would like to use 16 ADC0 Channels to be sensed using PDB0 Triggering. Thus I provide the delays as follows. I'm using FTM so as to trigger the PDB Channels. 


PDB0->CH[0].DLY[0] = 100; 
PDB0->CH[0].DLY[1] = 200; 
PDB0->CH[0].DLY[2] = 300; 
PDB0->CH[0].DLY[3] = 340; 
PDB0->CH[0].DLY[4] = 500; 
PDB0->CH[0].DLY[5] = 600; 
PDB0->CH[0].DLY[6] = 700; 
PDB0->CH[0].DLY[7] = 800; 

I need to raise an interrupt after 6 ADC sense (6th pre-trigger), but I'm getting a sequence error in this process.

I had the below questions.

1. Do we need to read the ADC Channels (0-7) after every Conversion so as to enable to COCO Flag again? as it mentioned in RM below. 

pastedImage_1.png

2. What is the minimum delay time between two pre-triggers?

Kindly help in this regard.

Thanks in advance,

Raju

0 项奖励
回复
1 解答
11,808 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) yes, you need to read the result so the COCO will be cleared and thus can be set again which makes a pretrigger lock inactive.

2) delay time between two pre-triggers must be ADC conversion time at least.  

See chapter 42.5.4.5 Sample time and total conversion time of the RM.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
19 回复数
11,809 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) yes, you need to read the result so the COCO will be cleared and thus can be set again which makes a pretrigger lock inactive.

2) delay time between two pre-triggers must be ADC conversion time at least.  

See chapter 42.5.4.5 Sample time and total conversion time of the RM.

BR, Petr

0 项奖励
回复
11,808 次查看
bjrajendra
Senior Contributor I

Hi Petr,

Can you suggest any other alternative to reading the ADC values after every pre-trigger, since I need to convert the values & also implement certain functionalities which takes a sufficient amount of time?

There will be a high chance of another pre-trigger appears before the completion of the function.

Raju.

0 项奖励
回复
11,808 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can try to use DMA to read a results, some examples are given here

Example S32K144 PDB ADC trigger DMA ISR S32DS 

https://community.nxp.com/docs/DOC-343295 

BR, Petr

0 项奖励
回复
11,808 次查看
bjrajendra
Senior Contributor I

Hi Petr,

Thanks for the reply.

I tried accessing those

Example S32K144 PDB ADC trigger DMA ISR S32DS  

   the link was deleted I guess and below is the display it's showing.

pastedImage_1.png

Example S32K144 PDB ADC DMA S32DS.ARM.2018.R1 

   the zip file doesn't contain any data

Raju

0 项奖励
回复
11,808 次查看
PetrS
NXP TechSupport
NXP TechSupport

I have uploaded the first one again, and see no issue with the second one.

BR, Petr

0 项奖励
回复
11,808 次查看
bjrajendra
Senior Contributor I

Hi Petr.

Thanks for your response.

I just downloaded Example S32K144 PDB ADC trigger DMA ISR S32DS and made suitable changes like clock and 42 (ADC0_COCO) DMAMUX source, everything works fine.

Now, I tried to add new TCD as I would like to use both ADC0 & ADC1. To make it simpler I just used only ADC1 not ADC0 with TCD[1] not TCD[0], so that later I can add both.

I just added a new function void DMA1_init(void) with all TCD[0] replaced with TCD[1] and new source & destination array. Also, I ensured the ADC1 with DMAEN.

Finally with void DMAMUX1_Init (void) --->
DMAMUX->CHCFG[1] |= DMAMUX_CHCFG_SOURCE(43);

Now my ISR is not executing. What changes I need to do so as to execute my isr ?

Kindly help in this regard.

Raju

0 项奖励
回复
11,808 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

not sure, are you able to share full example so this can be checked?

The SDK example I pointed last time is using both ADCs and DMAs are used to read them out, but probably you would like to have baremetal example.

BR, Petr

0 项奖励
回复
11,807 次查看
bjrajendra
Senior Contributor I

Hi Petr,

Thanks for your response.

As you told, I'm using bare metal example & trying to configure the new one.

Attached is the edited example which I downloaded.

Would like to know the reason why my ISR isn't executing.

Raju

0 项奖励
回复
11,807 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if the DMA ch1 is a source for interrupt in your modified code then correct interrupt init and interrupt vector have to be used. Try below code

void IRQs_Init (void)
{
   FSL_NVIC->ICPR[0] = 1 << (1 % 32); /* IRQ1-DMA ch1: clr any pending IRQ*/
   FSL_NVIC->ISER[0] = 1 << (1 % 32); /* RQ1-DMA ch1: enable IRQ */
   FSL_NVIC->IP[1] = 0xA; /* IRQ1-DMA ch1: priority 10 of 0-15*/
}


void DMA1_IRQHandler(void)
{

   PDB1->SC |= PDB_SC_SWTRIG_MASK; /* restart PDB counter */

   DMA->CINT = 1; // clear DMA channel 1 interrupt flag
}

BR, Petr

11,807 次查看
bjrajendra
Senior Contributor I

Hi Petr,

I had another question.

With back to back connection on all pdb channels but there is a trigger interrupt only for ADC_SC[8] still, there is a sequence error. But, will it affects other back to back triggers and its conversion as I would like to ignore the sequence error.

Kindly suggest the solution.

Raju

0 项奖励
回复
11,806 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

not sure of the overall configuration, but I assume that that the sequence error affects next back-to-back conversions on channel which indicate an error. And so you should resolve an error.

BR, Petr

0 项奖励
回复
11,806 次查看
bjrajendra
Senior Contributor I

Dear Petr,

Thanks for your feedback & it's really helpful.

As mentioned in the document, my calculation is as follows.

ADC TOTAL CONVERSION TIME = Sample Phase Time (set by SMPLTS + 1) + Hold Phase (1 ADC Cycle) + Compare Phase Time (8-bit Mode = 20 ADC Cycles, 10-bit Mode = 24 ADC Cycles, 12-bit Mode = 28 ADC Cycles) + Single or First continuous time adder (5 ADC cycles + 5 bus clock cycles)

i.e., for 12-bit conversion = (40+SMPLTS)/(fadc)

For our code SMPLTS=12. Therefore, conversion time = 53/40M =1.325us.

Considering that as conversion time if I keep PDB delay of 200 (200/80M=2.5us) between 0 & 1, I'm getting a sequence Error.

Am I correct in calculating the conversion time.

Kindly help in this regard.

Raju

0 项奖励
回复
11,806 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

calculation looks correct. Do you really have ADCK 40MHz, what is the clock source?

BR, Petr

0 项奖励
回复
11,806 次查看
bjrajendra
Senior Contributor I

I tried changing the delay value where it works 450 counts it means, it takes 450/80M = 5.625us.

5.625 means with clock 40MHz it takes 225 ADC cycles to convert.

Kindly suggest where I went wrong.

ADC initialization as follows.

pastedImage_1.png

Raju

0 项奖励
回复
11,807 次查看
PetrS
NXP TechSupport
NXP TechSupport

seems you have ADIV=2, so ADCK=10MHz

BR, Petr

0 项奖励
回复
11,807 次查看
bjrajendra
Senior Contributor I

Hi Petr,

Thanks for the solution. Forgot to change the setting after initializing for calibration.

With 40MHz setting & with PDB Clock 80MHz it requires 104 counts between two delays. I tried keeping 110 it didn't work but it worked with 120 count.

Can I know any possible reasons?

Raju

0 项奖励
回复
11,809 次查看
PetrS
NXP TechSupport
NXP TechSupport

I guess there will be additional clocks due to triggering...

BR, Petr

0 项奖励
回复
11,809 次查看
bjrajendra
Senior Contributor I

Dear Petr,

Thanks for your swift response.

I'm using PLLDIV2 which actually generates from 8MHZ External Oscillator & Below are my corresponding settings.

SCG->SPLLDIV = 0x00000302; /* SPLLDIV1 divide by 2; SPLLDIV2 divide by 4 */

PCC->PCCn[PCC_ADC0_INDEX] |= PCC_PCCn_PCS(6); /* PCS=6: Select SPLLDIV2_CLK=40MHz */

Raju

0 项奖励
回复
11,809 次查看
PetrS
NXP TechSupport
NXP TechSupport

OK, so if you read result registers and the period of FTM is enough for all conversions, then it should work.

If have troubles still please share your full setting/code.

BR, Petr 

0 项奖励
回复