Hi, I trying data send with dma as a scatter/gather. My purpose is to send data(for example a 120-byte array) with flexI2S.
I want dma to send the same array again when 120 bytes are finished automatically without any triggering in the loop while.
I reviewed the "edma_transfer_s32k146" project on S32DS. The project was not configured to send data from the flex module.
I cannot do what I am trying to do by setting the scatterGatherEnable variable to true and giving the scatterGatherNextDescAddr the address of the directory.
What do you think is missing in this program for what I want to do? (Does S32K116 processor have any restrictions to do this? Do you have a sample project that does this? It doesn't matter if it's FlexI2C, FlexSPI or something.)
In addition, I added configuration to flex module, like this:
Also, if I send the data with the "FLEXIO_I2S_DRV_MasterSendData" function after checking via FLEXIO_I2S_DRV_MasterGetStatus() in the while loop, the flex module sends the data successfully. But what I need is to create a seamless I2S clock signal.
已解决! 转到解答。
Hi @Furkan07,
Although the FlexIO SDK driver does not support it, the DMA channel can be triggered again at the end of the Major loop.
TCDn_CSR[MAJORLINKCH] can be set the n channel.
Regards,
Daniel
Hi @Furkan07,
Although the FlexIO SDK driver does not support it, the DMA channel can be triggered again at the end of the Major loop.
TCDn_CSR[MAJORLINKCH] can be set the n channel.
Regards,
Daniel
Yes, you are right. I was able re-trigger the DMA channel when the DMA data send finished for creating a continuous DMA transmission. Result; (blue: clk, yellow: data)
But it took some time to figure out how to do it. Even the simple process of sending a string continuously requires reading quite a few resources on the minor loop and the major loop. The fact that NXP doesn't do it as simply as in CUBE MX is challenging for NXP beginners.
@danielmartynek, Thank you for the reply.