[Security] Multiple Encryption/Decryption Interface Call Errors on D-Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Security] Multiple Encryption/Decryption Interface Call Errors on D-Flash

Jump to solution
2,744 Views
Gideon
Contributor III

Dear NXPs:

ARCH:S32K142

OS:None

IDE:IAR arm 9.32.2

Bootloader- D-Flash-32K

Background Reference:Solved: Re: [Security] D-Flash CSE driver encryption/decryption interface limitations - NXP Communit...

CSEc Driver uses S32K SDK driver.

After executing the encryption and decryption interface multiple times, a Hardfault error occurred.

IHPRECISERR = 1

FORCED = 1

Gideon_0-1721383057694.jpegGideon_1-1721383074701.jpeg

Test code:The encryption and decryption are called every 24ms, and a hardFault occurs after 42 executions.

Gideon_2-1721383162740.png

Q:It is speculated that it is related to the RAMization of the CSEC Driver function. How can I solve this problem?

 

 

0 Kudos
Reply
1 Solution
2,593 Views
Gideon
Contributor III

This matter has been resolved, this matter has been closed.

View solution in original post

0 Kudos
Reply
2 Replies
2,593 Views
Gideon
Contributor III

This matter has been resolved, this matter has been closed.

0 Kudos
Reply
2,718 Views
Gideon
Contributor III

Dear NXPS:

After executing S32_SCB->ACTLR |= S32_SCB_ACTLR_DISDEFWBUF_MASK;, the Hardfault type is determined.

Gideon_0-1721446777005.jpegGideon_1-1721446799680.jpeg

Sat Jul 20, 2024 11:26:34: HardFault:
Sat Jul 20, 2024 11:26:34: Forced escalated exception
Sat Jul 20, 2024 11:26:34: BusFault fault:
Sat Jul 20, 2024 11:26:34: Precise data error
Sat Jul 20, 2024 11:26:34: BFAR is valid
Sat Jul 20, 2024 11:26:34: Fault address BFAR: 0x12
Sat Jul 20, 2024 11:26:34: PC 0x10000b12
Sat Jul 20, 2024 11:26:34: SP 0x20002f50
Sat Jul 20, 2024 11:26:34: LR 0xffffffe9
Sat Jul 20, 2024 11:26:34: Vector table: 0x1fffc000
Sat Jul 20, 2024 11:26:34: Stopped by a vector catch:
Sat Jul 20, 2024 11:26:34: BusFault fault escalated into HardFault
Sat Jul 20, 2024 11:26:34: The BusFault handler is disabled
Sat Jul 20, 2024 11:26:34: HardFault exception.
Sat Jul 20, 2024 11:26:34: The processor has escalated a configurable-priority exception to HardFault.
Sat Jul 20, 2024 11:26:34:
Sat Jul 20, 2024 11:26:34: A precise data access error has occurred (CFSR.PRECISERR, BFAR)
Sat Jul 20, 2024 11:26:34: At data address 0x12.
Sat Jul 20, 2024 11:26:34:
Sat Jul 20, 2024 11:26:34: Exception occurred at PC = 0x100012ce, LR = 0x10000ee1
Sat Jul 20, 2024 11:26:34:
Sat Jul 20, 2024 11:26:34: See the call stack for more information.

As mentioned above, looking forward to your help.

 

 

 

 

0 Kudos
Reply