Need a help about SDK of S32K is the class of ASPICE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need a help about SDK of S32K is the class of ASPICE

Jump to solution
799 Views
boabo
Contributor I

Need a help about SDK of S32K is the class of ASPICE,thanks!

0 Kudos
Reply
1 Solution
776 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

See the description(A-SPICE) of the Software Quality Levels section of the S32 Software Development Kit - Fact Sheet

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
777 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

See the description(A-SPICE) of the Software Quality Levels section of the S32 Software Development Kit - Fact Sheet

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------