SPD BIST config question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPD BIST config question

ソリューションへジャンプ
3,078件の閲覧回数
Pusoy
Contributor III

Hi,

In the section of STCU2 in the "S32K3xx Reference Manual, Rev. 7,05/2023", there are some precautions before self-test.
For the two items circled in the image, I couldn't find the corresponding implementation code in the "

S32K3 Safety Peripheral Drivers version 1.0.3

"

.

Pusoy_1-1702623528440.png

 

1. Are these two parts implemented in the S32K3 Safety Peripheral Drivers?

2. If they are implemented, can you please help me locate them?

Thank you very much!

 

タグ(3)
0 件の賞賛
返信
1 解決策
3,039件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. Are these reset sources in table 287 automatically disabled by BIST after the user runs BIST_RUN?

Yes. I expect that hardly one of those modules can request reset in RGM while its content is filled with test patterns.

2. Similarly, regarding the second highlighted area about disabling communication peripherals, do we need to manually code the shutdown of these peripherals before running BIST_RUN?

Yes, this was the common practice.

However, such routines could be now part of SPD /SAF driver (I would expect that). Since I do not know SAF in details but I do have deep knowledge on STCU.

Anyway it should be in documentation to the SAF /SPD or in some precondition BIST functions.

Best regards,

Peter

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,040件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. Are these reset sources in table 287 automatically disabled by BIST after the user runs BIST_RUN?

Yes. I expect that hardly one of those modules can request reset in RGM while its content is filled with test patterns.

2. Similarly, regarding the second highlighted area about disabling communication peripherals, do we need to manually code the shutdown of these peripherals before running BIST_RUN?

Yes, this was the common practice.

However, such routines could be now part of SPD /SAF driver (I would expect that). Since I do not know SAF in details but I do have deep knowledge on STCU.

Anyway it should be in documentation to the SAF /SPD or in some precondition BIST functions.

Best regards,

Peter

 

0 件の賞賛
返信
3,053件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

FCCU RST is disabled by the BIST as description express:

petervlna_0-1702886102423.png

Second the corresponding PCTLs can be controlled by ME module. basically the note ask you to disable clocks to peripherals before test is started.

This is most probably implemented by BASE module of AUTOSAR drivers. I do not expect that this is the part of SDP driver as it is general Mode entry functionality.

For details refer to reference manual : 47.1.4 Core clock gating

petervlna_3-1702888459724.png

 

petervlna_1-1702887969159.png

For example:

petervlna_2-1702887980358.png

Best regards,

Peter

 

 

 

0 件の賞賛
返信
3,041件の閲覧回数
Pusoy
Contributor III

Hello Peter,

Thank you very much for your reply. I apologize if my previous questions were not clear. I still have two questions that I haven't understood clearly:

1. Are these reset sources in table 287 automatically disabled by BIST after the user runs BIST_RUN?
2. Similarly, regarding the second highlighted area about disabling communication peripherals, do we need to manually code the shutdown of these peripherals before running BIST_RUN?

I look forward to your reply. Thank you!

Pusoy_0-1702965820347.png

 

0 件の賞賛
返信