SENT TX emulation using FLEXIO or EMIOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SENT TX emulation using FLEXIO or EMIOS

1,555 Views
UmaMaheswaraReddy
Contributor IV

Hi,

We need pulse width measurement feature and PWM generation feature on same pin. Is FLEXIO or EMIOS which is best suit for this need?

Can we measure pulse width using FLEXIO input capture? We are planning to use FLEXIO module as a SPC SENT transmitter emulator. In SENT SPC after receiving trigger pulse we will start sent transmission, as per the requirement I need to measure the trigger pulse width.

Below is the trigger pulse sample. Can we measure below pulse width using FLEXIO input capture mode?

UmaMaheswaraReddy_0-1732349136947.png

Thanks,

Y Uma Maheswara Reddy.

 

 

0 Kudos
Reply
1 Reply

1,213 Views
Dinesh_Guleria
NXP Employee
NXP Employee

Hi @UmaMaheswaraReddy ,


>> We need pulse width measurement feature and PWM generation feature on same pin. Is FLEXIO or EMIOS which is best suit for this need?
Please find example using EMIOS.

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-cap...

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-cap...

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-PWM-ICU-using-EMIOS-DS3-5-RTD300...

For sent please create separate ticket so that we can assign it to right person.

Regards,
Dinesh

0 Kudos
Reply