S32k flexIO shifter match store mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32k flexIO shifter match store mode

跳至解决方案
2,692 次查看
yuegao1996
Contributor II

Hi,

      in match store mode,  the manual says higher 16 bits are used to set the data to be matched and the lower to mask the results.  Since the shifter is 32bit, so how does it be compared to SHIFTBUF[31:16], and how data is received when a match occurs? 

 

BR

 

0 项奖励
回复
1 解答
2,678 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

       yes, I think it should be like this.

      The step"n+2"  says: "when match occur store shifter data into the buffer, and set some flag bit".

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,685 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

      You can refer to the process in the figure below.

Senlent_0-1630464166985.png

BR!

      Jim,

0 项奖励
回复
2,681 次查看
yuegao1996
Contributor II

Hi Jim, 

does this mean that as far as the higher 16 bits matched, then the whole 32 bit data in the shifter will be loaded to the shiftbuf?

 

many thanks,

Yuri

0 项奖励
回复
2,679 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

       yes, I think it should be like this.

      The step"n+2"  says: "when match occur store shifter data into the buffer, and set some flag bit".

0 项奖励
回复