S32k flexIO shifter match store mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k flexIO shifter match store mode

ソリューションへジャンプ
2,686件の閲覧回数
yuegao1996
Contributor II

Hi,

      in match store mode,  the manual says higher 16 bits are used to set the data to be matched and the lower to mask the results.  Since the shifter is 32bit, so how does it be compared to SHIFTBUF[31:16], and how data is received when a match occurs? 

 

BR

 

0 件の賞賛
返信
1 解決策
2,672件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

       yes, I think it should be like this.

      The step"n+2"  says: "when match occur store shifter data into the buffer, and set some flag bit".

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,679件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

      You can refer to the process in the figure below.

Senlent_0-1630464166985.png

BR!

      Jim,

0 件の賞賛
返信
2,675件の閲覧回数
yuegao1996
Contributor II

Hi Jim, 

does this mean that as far as the higher 16 bits matched, then the whole 32 bit data in the shifter will be loaded to the shiftbuf?

 

many thanks,

Yuri

0 件の賞賛
返信
2,673件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

       yes, I think it should be like this.

      The step"n+2"  says: "when match occur store shifter data into the buffer, and set some flag bit".

0 件の賞賛
返信