Hi everyone.
Does NXP have a "IEC60730 class B safety solution" for S32K14X series?
I found some "ISO26262-compliant core test solutions", but not having a same coverage with "IEC60730 class B"
Is it possible to use the safety library captured below for S32K14X series also?
Best Regards,
Sunghou
Hi @sunghou,
Unfortunately, the IEC60730 libraries are not available for the S32K144 device.
https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTN...
There is a private SafeAssure community group with all the available safety documentation.
The community group is monitored daily by our experts on application safety.
https://community.nxp.com/groups/safeassure-nda
An NDA is required:
https://community.nxp.com/docs/DOC-335524
Regards,
Daniel
Hi,danielmartynek
Can the source code of iec60730b safety library for CM4 version 4.1 be provided to us?