S32k flexIO shifter match store mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k flexIO shifter match store mode

Jump to solution
2,710 Views
yuegao1996
Contributor II

Hi,

      in match store mode,  the manual says higher 16 bits are used to set the data to be matched and the lower to mask the results.  Since the shifter is 32bit, so how does it be compared to SHIFTBUF[31:16], and how data is received when a match occurs? 

 

BR

 

0 Kudos
Reply
1 Solution
2,696 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

       yes, I think it should be like this.

      The step"n+2"  says: "when match occur store shifter data into the buffer, and set some flag bit".

View solution in original post

0 Kudos
Reply
3 Replies
2,703 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

      You can refer to the process in the figure below.

Senlent_0-1630464166985.png

BR!

      Jim,

0 Kudos
Reply
2,699 Views
yuegao1996
Contributor II

Hi Jim, 

does this mean that as far as the higher 16 bits matched, then the whole 32 bit data in the shifter will be loaded to the shiftbuf?

 

many thanks,

Yuri

0 Kudos
Reply
2,697 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

       yes, I think it should be like this.

      The step"n+2"  says: "when match occur store shifter data into the buffer, and set some flag bit".

0 Kudos
Reply