S32K3XX DMA Error Interrupt not visible in INT register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3XX DMA Error Interrupt not visible in INT register

Jump to solution
1,065 Views
RafalK
Contributor II

Hello,

DMA error interrupt seems to not set  CHn_INT[INT] register when triggered.

I configured DMA to work LPSPI on S32K396 EVB and it is working fine. However I wanted to test DMA error handling so I corrupted DMA TCD source address by setting some invalid address.

This is causing DMA channel interrupt to be triggered (I'm using Channel 14 from DMAMUX).

I can see that ERR and SBE bits are set so error was catched correctly and interrupt handler was called for this channel but INT register is zero (see attachment).

According to manual INT register should be set for INTHALF, INTMAJOR and EEI interrupt events.

INTMAJOR event is working but EEI is not.

Am I missing something?

0 Kudos
Reply
1 Solution
1,025 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

INT and INT_ERR are different interrupt events, it is correct that INT flag is not set in this case.

davidtosenovjan_0-1733309563558.png

It is following field in 14.6.2.3 Channel Error Status (CH0_ES - CH31_ES) supposing to be set (and cleared by w1c during ISR):

davidtosenovjan_0-1733310127190.png

 

 

 

 

View solution in original post

0 Kudos
Reply
1 Reply
1,026 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

INT and INT_ERR are different interrupt events, it is correct that INT flag is not set in this case.

davidtosenovjan_0-1733309563558.png

It is following field in 14.6.2.3 Channel Error Status (CH0_ES - CH31_ES) supposing to be set (and cleared by w1c during ISR):

davidtosenovjan_0-1733310127190.png

 

 

 

 

0 Kudos
Reply