S32K3XX DMA Error Interrupt not visible in INT register

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3XX DMA Error Interrupt not visible in INT register

跳至解决方案
1,095 次查看
RafalK
Contributor II

Hello,

DMA error interrupt seems to not set  CHn_INT[INT] register when triggered.

I configured DMA to work LPSPI on S32K396 EVB and it is working fine. However I wanted to test DMA error handling so I corrupted DMA TCD source address by setting some invalid address.

This is causing DMA channel interrupt to be triggered (I'm using Channel 14 from DMAMUX).

I can see that ERR and SBE bits are set so error was catched correctly and interrupt handler was called for this channel but INT register is zero (see attachment).

According to manual INT register should be set for INTHALF, INTMAJOR and EEI interrupt events.

INTMAJOR event is working but EEI is not.

Am I missing something?

0 项奖励
回复
1 解答
1,055 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

INT and INT_ERR are different interrupt events, it is correct that INT flag is not set in this case.

davidtosenovjan_0-1733309563558.png

It is following field in 14.6.2.3 Channel Error Status (CH0_ES - CH31_ES) supposing to be set (and cleared by w1c during ISR):

davidtosenovjan_0-1733310127190.png

 

 

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,056 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

INT and INT_ERR are different interrupt events, it is correct that INT flag is not set in this case.

davidtosenovjan_0-1733309563558.png

It is following field in 14.6.2.3 Channel Error Status (CH0_ES - CH31_ES) supposing to be set (and cleared by w1c during ISR):

davidtosenovjan_0-1733310127190.png

 

 

 

 

0 项奖励
回复