S32K358 Pin Drive strength

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K358 Pin Drive strength

ソリューションへジャンプ
2,845件の閲覧回数
Changwoo82
Contributor II

Hello.

I'm configuring the pins for LPSPI0 like below.

How can I find the drive strength setting for each pin in the source code or Design Studio?

In Design Studio, it is impossible to set the driver strength.

moyu82_0-1699012849596.png

Are there any options to set this? These pins just set as defined in the datasheet?

ex) PTE4: Standard, PTE1: Standard, PTE0: Standard, PTE2: Standard

 

Thank you

0 件の賞賛
返信
1 解決策
2,830件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Changwoo82 

The pins that support High-Drive strength depend on the pad type. As you mentioned, all the LPSPI pins selected are standard and do not support it, so it is not possible to enable it in the Pin Tool. 

VaneB_0-1699052208747.png

B.R.

VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,831件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Changwoo82 

The pins that support High-Drive strength depend on the pad type. As you mentioned, all the LPSPI pins selected are standard and do not support it, so it is not possible to enable it in the Pin Tool. 

VaneB_0-1699052208747.png

B.R.

VaneB

0 件の賞賛
返信
2,797件の閲覧回数
Changwoo82
Contributor II
Thank you!
0 件の賞賛
返信