S32K358 Pin Drive strength

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K358 Pin Drive strength

Jump to solution
2,825 Views
Changwoo82
Contributor II

Hello.

I'm configuring the pins for LPSPI0 like below.

How can I find the drive strength setting for each pin in the source code or Design Studio?

In Design Studio, it is impossible to set the driver strength.

moyu82_0-1699012849596.png

Are there any options to set this? These pins just set as defined in the datasheet?

ex) PTE4: Standard, PTE1: Standard, PTE0: Standard, PTE2: Standard

 

Thank you

0 Kudos
Reply
1 Solution
2,810 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Changwoo82 

The pins that support High-Drive strength depend on the pad type. As you mentioned, all the LPSPI pins selected are standard and do not support it, so it is not possible to enable it in the Pin Tool. 

VaneB_0-1699052208747.png

B.R.

VaneB

View solution in original post

0 Kudos
Reply
2 Replies
2,811 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Changwoo82 

The pins that support High-Drive strength depend on the pad type. As you mentioned, all the LPSPI pins selected are standard and do not support it, so it is not possible to enable it in the Pin Tool. 

VaneB_0-1699052208747.png

B.R.

VaneB

0 Kudos
Reply
2,777 Views
Changwoo82
Contributor II
Thank you!
0 Kudos
Reply