S32K344 use TJA1153 send can message fail problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K344 use TJA1153 send can message fail problem

跳至解决方案
2,150 次查看
tianxing
Contributor IV

I made a program with flexcan sdk and I debug on the EVB.

The program can send can message but not all the time .

For example the first time download elf file and run can send the can message successful but the second time download elf file and run cannot send the can message.

Why this happened? Please help me solve this problem.

And the attach file is the program.

0 项奖励
回复
1 解答
2,136 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could below thread be useful for you?

https://community.nxp.com/t5/S32K/S32K344-Evaluation-Board-FlexCan-Example-running/m-p/1343355

If using S32K3X4EVB-Q257, there is secure CAN transceiver on the board, TJA1153, which is not configured by default and it does not allow the MCU to communicate with the CAN bus. So a config must be done first.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,137 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could below thread be useful for you?

https://community.nxp.com/t5/S32K/S32K344-Evaluation-Board-FlexCan-Example-running/m-p/1343355

If using S32K3X4EVB-Q257, there is secure CAN transceiver on the board, TJA1153, which is not configured by default and it does not allow the MCU to communicate with the CAN bus. So a config must be done first.

BR, Petr

0 项奖励
回复
2,119 次查看
tianxing
Contributor IV

Thank you the problem is solved

0 项奖励
回复