S32K344 use TJA1153 send can message fail problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 use TJA1153 send can message fail problem

Jump to solution
2,120 Views
tianxing
Contributor IV

I made a program with flexcan sdk and I debug on the EVB.

The program can send can message but not all the time .

For example the first time download elf file and run can send the can message successful but the second time download elf file and run cannot send the can message.

Why this happened? Please help me solve this problem.

And the attach file is the program.

0 Kudos
Reply
1 Solution
2,106 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could below thread be useful for you?

https://community.nxp.com/t5/S32K/S32K344-Evaluation-Board-FlexCan-Example-running/m-p/1343355

If using S32K3X4EVB-Q257, there is secure CAN transceiver on the board, TJA1153, which is not configured by default and it does not allow the MCU to communicate with the CAN bus. So a config must be done first.

BR, Petr

View solution in original post

0 Kudos
Reply
2 Replies
2,107 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could below thread be useful for you?

https://community.nxp.com/t5/S32K/S32K344-Evaluation-Board-FlexCan-Example-running/m-p/1343355

If using S32K3X4EVB-Q257, there is secure CAN transceiver on the board, TJA1153, which is not configured by default and it does not allow the MCU to communicate with the CAN bus. So a config must be done first.

BR, Petr

0 Kudos
Reply
2,089 Views
tianxing
Contributor IV

Thank you the problem is solved

0 Kudos
Reply