Hello NXP Team.
I tried configuring SPI, CPOL = 1 ,CPHA = 1.
The waveform is correct when i use 100K baudreate,
But when i use 1M baudrate, the waveform will be wrong.
Usually, data error will occur after the data pin maintains a high voitage for a long time.
Baudrate 100k
Baudrate 1M
The following is my project
Thank you
解決済! 解決策の投稿を見る。
Hello @IanHsueh.
I tested your project on my side without any modifications, connecting the MOSI to the MISO to verify if the data was transmitted correctly despite the analyzer's information. I successfully received in the buffer the correct data. Could you please do perform the same test? This will help us rule out any potential issues with the logic analyzer, as we have encountered problems with them when observing a data frame.
Also, let me know if the tests were done in a custom board or in one of our evaluation boards.
I will be waiting for your answer.
- RomanVR.
Hello @RomanVR ,after a few days of testing, i found that it seems to be a problem with the C code of main.c
Thank you for informing us that you've identified the issue.
If you have any further questions or encounter any other unresolved issues, please feel free to reach out.
- RomanVR.
Hello @RomanVR ,thank for ur reply
I don't know how to connect MOSI to MISO to verify the data, is there any instructions?
And I'm running on this board.
btw, I used the example on this webpage(used LSPI2, without dma), deleted the configuration, used 1M baudrate, and tested it. The waveform was correct.
Example S32K344 SPI Transmit & Receive Using DMA DS3.5 RTD500 - NXP Community
The following is an example of my modification. I compared the SPI and PORT settings and they are consistent. I don't know what went wrong with the project I created.
Hello @IanHsueh.
I tested your project on my side without any modifications, connecting the MOSI to the MISO to verify if the data was transmitted correctly despite the analyzer's information. I successfully received in the buffer the correct data. Could you please do perform the same test? This will help us rule out any potential issues with the logic analyzer, as we have encountered problems with them when observing a data frame.
Also, let me know if the tests were done in a custom board or in one of our evaluation boards.
I will be waiting for your answer.
- RomanVR.