Hello
When I was using S32K344 to test the data read and write of DataFlash, I found that if the same ECC area (8 bytes) was programmed multiple times, it would cause ECC errors and trigger HardFault interrupts.
1. How can I distinguish between ECC error interrupts and HardFault interrupts, that is, call another interrupt function when an ECC error occurs
2. Do you have sample software for ECC? I am not sure what kind of processing the software should do after triggering ECC
BestRegards,
Simon
已解决! 转到解答。
Hello, @danielmartynek
In the sample software, I saw the following operations performed in the HardFault_Handler process:
1. Clear the fault flag and bus fault address register
2. Clear the ECC error flag of the MCRS register
3. Move the stack pointer backward to skip the instruction address where the ECC error occurred
1 and 2 above are to clear the error flag, and 3 is to prevent the error interrupt from being triggered again after the interrupt processing is completed. Is my understanding correct?
BestRegards,
Simon