S32K344 - Example Code for EMAC HW-IP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K344 - Example Code for EMAC HW-IP

2,378 次查看
mrtientv6
Contributor II

Hi experts,

We are using S32K3X4EVB-T172 Evaluation Board, but I cannot find example code for Ethernet (EMAC) in RTD package. I only see GMAC example.

Could you please share where can I get example code of EMAC?

Thanks,

Tien

2 回复数

2,338 次查看
Nhi_Nguyen
NXP Employee
NXP Employee

Hi Tien,

Why did you think that example is for GMAC not EMAC.

You can see as below:

Nhi_Nguyen_0-1690791499360.pngNhi_Nguyen_0-1690791499360.png

Nhi_Nguyen_1-1690791508466.pngNhi_Nguyen_1-1690791508466.png

This means that S32K344 just supports EMAC not GMAC and the example S32K344 was attached in the package is for EMAC not GMAC.

Best regards,

Nhi

 

0 项奖励
回复

2,330 次查看
mrtientv6
Contributor II

Hi @Nhi_Nguyen 

 

Thank you for your support.

In RTD package, I only see GMAC in plugin name of ETH:

mrtientv6_0-1690795638639.pngmrtientv6_0-1690795638639.png

 

But this supported EMAC HW also.

Thanks,

0 项奖励
回复