Hello,
Can anyone please tell me how to check TJA1153 is in Vanilla state? I tried searching for datasheet of TJA1153 on internet but couldn't able to find it.
BR,
Ajay
Hi,
do you see timeElapsed increasing so can pass mS2Ticks in case MB flag is not set?
BR, Petr
yes increasing , Im sure the issue is related to TJA1153 but I couldn't find a solution.
Hi,
if increasing then function does not block but should return FLEXCAN_STATUS_TIMEOUT after while if message is not transmitted successfully.
If the communication itself is not working, it could be due to TJA1153. If this is in Vanilla state, it must go through power on to be able to configure it.
BR, Petr
Hello everybody !
I have the same issue. Could anybody help to figure this out?
Thx