S32K312-sleep problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312-sleep problem

Jump to solution
3,649 Views
Simon_Liu
Contributor II

Background:
1. Use the S32Design Studio tool to import the example [Power_Ip_Example_S32K312], and additionally configure the STANDBY mode.
2. Added Wkpu in Drivers and configured PTB19 as the wakeup source, and configured related Wkp interrupt.
3. Configure PTE18 as GPIO output

Operation:
1. Perform Power initialization, Siul2 initialization, wkp initialization, interrupt enable, etc. in the Main function.
2. Set PTE18 as high level output.
3. 3. Call the Power_Ip_SetMode function to pass in the StandBy parameters.

Problems:
1. PTE18 does not change to low level after StandBy.
2. The current does not drop significantly after StandBy.

What are the reasons for the above two questions?

0 Kudos
Reply
1 Solution
3,584 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@SimonLiu93

if padkeeping is disabled, the pin will remain the run mode after entering standby mode, but once it wakeups, the pin will become floating until initialized by software again.

View solution in original post

0 Kudos
Reply
4 Replies
3,623 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@SimonLiu93

would you please take a look at this post, it might be help you.

https://community.nxp.com/t5/S32K/about-S32K312-STANDBY-CURRENT/td-p/1654304 

0 Kudos
Reply
3,590 Views
Simon_Liu
Contributor II

Hi @Senlent 

Thank you for your answer.

Regarding the first question, after entering StandBy, if PadKeeping is not set, will the output pad level be maintained?

0 Kudos
Reply
3,585 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@SimonLiu93

if padkeeping is disabled, the pin will remain the run mode after entering standby mode, but once it wakeups, the pin will become floating until initialized by software again.

0 Kudos
Reply
3,574 Views
Simon_Liu
Contributor II

Hi @Senlent 

Thank you for your answer

0 Kudos
Reply