S32K312-sleep problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K312-sleep problem

跳至解决方案
3,646 次查看
Simon_Liu
Contributor II

Background:
1. Use the S32Design Studio tool to import the example [Power_Ip_Example_S32K312], and additionally configure the STANDBY mode.
2. Added Wkpu in Drivers and configured PTB19 as the wakeup source, and configured related Wkp interrupt.
3. Configure PTE18 as GPIO output

Operation:
1. Perform Power initialization, Siul2 initialization, wkp initialization, interrupt enable, etc. in the Main function.
2. Set PTE18 as high level output.
3. 3. Call the Power_Ip_SetMode function to pass in the StandBy parameters.

Problems:
1. PTE18 does not change to low level after StandBy.
2. The current does not drop significantly after StandBy.

What are the reasons for the above two questions?

0 项奖励
回复
1 解答
3,581 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@SimonLiu93

if padkeeping is disabled, the pin will remain the run mode after entering standby mode, but once it wakeups, the pin will become floating until initialized by software again.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,620 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@SimonLiu93

would you please take a look at this post, it might be help you.

https://community.nxp.com/t5/S32K/about-S32K312-STANDBY-CURRENT/td-p/1654304 

0 项奖励
回复
3,587 次查看
Simon_Liu
Contributor II

Hi @Senlent 

Thank you for your answer.

Regarding the first question, after entering StandBy, if PadKeeping is not set, will the output pad level be maintained?

0 项奖励
回复
3,582 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@SimonLiu93

if padkeeping is disabled, the pin will remain the run mode after entering standby mode, but once it wakeups, the pin will become floating until initialized by software again.

0 项奖励
回复
3,571 次查看
Simon_Liu
Contributor II

Hi @Senlent 

Thank you for your answer

0 项奖励
回复