S32K312 LPUART Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 LPUART Problem

1,138 Views
xingjunwei
Contributor I

when i send data use :

Lpuart_Uart_Ip_AsyncSend(UART2,frm->write_array, NEX13120_LEN_Write_data_Length1);

the MCU will enter :undefined_handler.

xingjunwei_0-1727418297734.pngxingjunwei_0-1727418297734.png

 

0 Kudos
Reply
1 Reply

1,117 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the examples:
Example S32K312 UART Transmit & Receive Using Interrupt DS3.5 RTD300
Example S32K312 UART Transmit & Receive Using DMA DS3.5 RTD300


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply