S32K324 Single and specific Core Reset issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K324 Single and specific Core Reset issue

1,233件の閲覧回数
ivaneo1979
Contributor I

Good morning,

I´m exploring the possibility to re-start a specific core, i.e. the main core wants to stop and completely restart the application core.

I successfully implemented both Application core initialization process and the Application Core shutdown process (46.1.6/7 in S32K3xx Ref.Manual).

This means that Core 0 can start Core 1 and can Stop it. 

However what I need is the possibility to completely restart the Core 1 after stopping it.

Try to explain: Core 1 Stop means that it remains in "standby" and waiting-for-interrupt (WFI), once this is triggered it carries on with the normal runtime flow BUT what I need it is to completely restart Core 1, i.e. I need a clean reset of a single Core.

Is that possible? I couldn´t find any way so far to implement this feature.

タグ(2)
0 件の賞賛
返信
1 返信

1,203件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ivaneo1979,

I see you have also created an internal case. I will continue to support you through the case in order to avoid any confusions.

Best regards,
Julián

0 件の賞賛
返信