S32K3 SPD compatibility with S32 Design Studio version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 SPD compatibility with S32 Design Studio version

Jump to solution
3,314 Views
Li_Chen
Contributor III

I have checked S32K3_SPD_1.0.3_ReleaseNotes.txt from S32 Safety Software Framework (SAF) and Safety Peripheral Drivers (SPD) | NXP Semiconductors, the release note said "Install the latest version of S32 Design Studio for S32 platform (currently v.3.5 SP1)". Our project is using S32DS 3.4 and RTD 2.0.0.

In order to integrate with SPD, do we need to upgrade S32DS IDE? Any migration guidance to move from old S32DS and RTD version to new ones?

0 Kudos
Reply
1 Solution
3,288 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If your project is development with S32DS v3.4 and S32K3 RTD 2.0.0, then you'd better download S32K3 Safety Peripheral Drivers version 1.0.2.

S32K3 Safety Peripheral Drivers version 1.0.2.png

S32K3_SPD_1.0.3_ReleaseNotes.txt mentioned that S32DS v3.5 SP1+S32K3 RTD 3.0.0 or 3.0.0 P07 is required. If you install S32K3 Safety Peripheral Drivers version 1.0.3, you may need to reconfigure in S32DS v3.5 referring to the S32Configuration Tool of the original project. 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
3,289 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If your project is development with S32DS v3.4 and S32K3 RTD 2.0.0, then you'd better download S32K3 Safety Peripheral Drivers version 1.0.2.

S32K3 Safety Peripheral Drivers version 1.0.2.png

S32K3_SPD_1.0.3_ReleaseNotes.txt mentioned that S32DS v3.5 SP1+S32K3 RTD 3.0.0 or 3.0.0 P07 is required. If you install S32K3 Safety Peripheral Drivers version 1.0.3, you may need to reconfigure in S32DS v3.5 referring to the S32Configuration Tool of the original project. 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,254 Views
Li_Chen
Contributor III

How about S32K3_SAF_1.0.3_EVAL_DS? I'd like to review the SAF package but I cannot find 1.0.2 version or older ones compatible with S32 Design Studio 3.4.

 

Thanks!

0 Kudos
Reply
3,235 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Here are the release notes of S32K3 SAF:

S32K3 SAF ReleaseNotes.png

S32K3_SAF_1.0.3: S32K3 RTD 3.0.0 or 3.0.0 P07 + S32DS v3.5. Have you contacted Distributor Network to inquire about the availability of different versions of S32K3 Safety Software Framework?

0 Kudos
Reply