S32K3 SPD compatibility with S32 Design Studio version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 SPD compatibility with S32 Design Studio version

ソリューションへジャンプ
880件の閲覧回数
Li_Chen
Contributor III

I have checked S32K3_SPD_1.0.3_ReleaseNotes.txt from S32 Safety Software Framework (SAF) and Safety Peripheral Drivers (SPD) | NXP Semiconductors, the release note said "Install the latest version of S32 Design Studio for S32 platform (currently v.3.5 SP1)". Our project is using S32DS 3.4 and RTD 2.0.0.

In order to integrate with SPD, do we need to upgrade S32DS IDE? Any migration guidance to move from old S32DS and RTD version to new ones?

0 件の賞賛
返信
1 解決策
854件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If your project is development with S32DS v3.4 and S32K3 RTD 2.0.0, then you'd better download S32K3 Safety Peripheral Drivers version 1.0.2.

S32K3 Safety Peripheral Drivers version 1.0.2.png

S32K3_SPD_1.0.3_ReleaseNotes.txt mentioned that S32DS v3.5 SP1+S32K3 RTD 3.0.0 or 3.0.0 P07 is required. If you install S32K3 Safety Peripheral Drivers version 1.0.3, you may need to reconfigure in S32DS v3.5 referring to the S32Configuration Tool of the original project. 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
855件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If your project is development with S32DS v3.4 and S32K3 RTD 2.0.0, then you'd better download S32K3 Safety Peripheral Drivers version 1.0.2.

S32K3 Safety Peripheral Drivers version 1.0.2.png

S32K3_SPD_1.0.3_ReleaseNotes.txt mentioned that S32DS v3.5 SP1+S32K3 RTD 3.0.0 or 3.0.0 P07 is required. If you install S32K3 Safety Peripheral Drivers version 1.0.3, you may need to reconfigure in S32DS v3.5 referring to the S32Configuration Tool of the original project. 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
820件の閲覧回数
Li_Chen
Contributor III

How about S32K3_SAF_1.0.3_EVAL_DS? I'd like to review the SAF package but I cannot find 1.0.2 version or older ones compatible with S32 Design Studio 3.4.

 

Thanks!

0 件の賞賛
返信
801件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Here are the release notes of S32K3 SAF:

S32K3 SAF ReleaseNotes.png

S32K3_SAF_1.0.3: S32K3 RTD 3.0.0 or 3.0.0 P07 + S32DS v3.5. Have you contacted Distributor Network to inquire about the availability of different versions of S32K3 Safety Software Framework?

0 件の賞賛
返信