S32K3 Linker Files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 Linker Files

Jump to solution
1,740 Views
1123HENRY
Contributor I

When I was using the S32K3 chip, I found that there was no linker_ram in the Linker Files folder

1123HENRY_0-1746584921677.png1123HENRY_0-1746584921677.png

S32K3 

 

0 Kudos
Reply
1 Solution
1,715 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @1123HENRY 

I can see that RTD examples does not have RAM target defined for some reasons. But if you create new application project with or without RTD then there are both RAM and flash targets.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
2 Replies
1,716 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @1123HENRY 

I can see that RTD examples does not have RAM target defined for some reasons. But if you create new application project with or without RTD then there are both RAM and flash targets.

Regards,

Lukas

0 Kudos
Reply
1,705 Views
1123HENRY
Contributor I
By creating a new project, I obtained the ld file of ram,thanks
0 Kudos
Reply