S32K3 Linker Files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,739件の閲覧回数
1123HENRY
Contributor I

When I was using the S32K3 chip, I found that there was no linker_ram in the Linker Files folder

1123HENRY_0-1746584921677.png1123HENRY_0-1746584921677.png

S32K3 

 

0 件の賞賛
返信
1 解決策
1,714件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @1123HENRY 

I can see that RTD examples does not have RAM target defined for some reasons. But if you create new application project with or without RTD then there are both RAM and flash targets.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,715件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @1123HENRY 

I can see that RTD examples does not have RAM target defined for some reasons. But if you create new application project with or without RTD then there are both RAM and flash targets.

Regards,

Lukas

0 件の賞賛
返信
1,704件の閲覧回数
1123HENRY
Contributor I
By creating a new project, I obtained the ld file of ram,thanks
0 件の賞賛
返信