S32K148EVB-Q176 Development Kit is not recognized by PC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K148EVB-Q176 Development Kit is not recognized by PC

跳至解决方案
2,132 次查看
CanCan
Contributor I

I have S32K148EVB-Q176 Development Kit and I am trying to connect it to my PC via its micro-USB port. But my PC does not even recognize that something is plugged to its USB port. I checked if I had any restrictions on my ports. I do not. I adjusted the pin configurations so that it takes the power from usb but still nothing. What should I do ?

0 项奖励
回复
1 解答
2,077 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @CanCan 

Thank you for the information.

Do you have an external debugger? This way you can try to connect to the evaluation kit and verify if the problem is from the S32K148 or the integrated debugger.

Miguel.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,090 次查看
CanCan
Contributor I

Hi @Miguel04,

I checked the configurations and my jumper configurations are as shown in the guide. I also tried to connect to my PC using the provided cable and with another one. Is there a possibilty that my micro-usb port is damaged and not working? I do not recognize that I've been harsh to the board. It feels that that is a low possibilty.

 

0 项奖励
回复
2,078 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @CanCan 

Thank you for the information.

Do you have an external debugger? This way you can try to connect to the evaluation kit and verify if the problem is from the S32K148 or the integrated debugger.

Miguel.

0 项奖励
回复
1,869 次查看
CanCan
Contributor I

Problem has solved. Thanks for the help

0 项奖励
回复
2,113 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @CanCan 

I would like to confirm that the jumper configuration of your S32K148EVB-Q176 correct.

Please look into this Getting started guide and compare the configuration of Step 3.1 Set Up Jumpers with your own.

Best Regards, Miguel.

 

0 项奖励
回复