S32K148EVB-Q176 Development Kit is not recognized by PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148EVB-Q176 Development Kit is not recognized by PC

ソリューションへジャンプ
3,059件の閲覧回数
CanCan
Contributor I

I have S32K148EVB-Q176 Development Kit and I am trying to connect it to my PC via its micro-USB port. But my PC does not even recognize that something is plugged to its USB port. I checked if I had any restrictions on my ports. I do not. I adjusted the pin configurations so that it takes the power from usb but still nothing. What should I do ?

0 件の賞賛
返信
1 解決策
3,004件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @CanCan 

Thank you for the information.

Do you have an external debugger? This way you can try to connect to the evaluation kit and verify if the problem is from the S32K148 or the integrated debugger.

Miguel.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,017件の閲覧回数
CanCan
Contributor I

Hi @Miguel04,

I checked the configurations and my jumper configurations are as shown in the guide. I also tried to connect to my PC using the provided cable and with another one. Is there a possibilty that my micro-usb port is damaged and not working? I do not recognize that I've been harsh to the board. It feels that that is a low possibilty.

 

0 件の賞賛
返信
3,005件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @CanCan 

Thank you for the information.

Do you have an external debugger? This way you can try to connect to the evaluation kit and verify if the problem is from the S32K148 or the integrated debugger.

Miguel.

0 件の賞賛
返信
2,796件の閲覧回数
CanCan
Contributor I

Problem has solved. Thanks for the help

0 件の賞賛
返信
3,040件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @CanCan 

I would like to confirm that the jumper configuration of your S32K148EVB-Q176 correct.

Please look into this Getting started guide and compare the configuration of Step 3.1 Set Up Jumpers with your own.

Best Regards, Miguel.

 

0 件の賞賛
返信