S32K148 LPSPI AUTOPCS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 LPSPI AUTOPCS

4,682件の閲覧回数
SONGTAOSI
Contributor I

Hi,

I counfig LPSPI1 as slave, LPSPI0 as master ,and LPSPI0 transfer data to LPSPI1,and LPSPI1_AUTOPCS bit is set,   TCR[CPHA]=1.The SCK(LPAPI0 produce )remain more than 4 LPSPI clock cycle between word. But when i do not connect LPSPI0_PCS0 to LPSPI1_PCS0, the transfer between LPSPI0 and LPSPI1 is failure,LPSPI1 can't receve data which from LPSPI0. 

Whether my understand correctly about ?  :  LPSPI1_AUTOPCS = 1,and TCR[CPHA]=1,andThe SCK(LPAPI0 produce )remain more than 4 LPSPI clock cycle between word. If the above conditions are met,Even if the LPSPI1_PCS0 not connect to LPSPI0_PCS0,LPSPI can receve data from LPSPI0.

ooking forward to your reply!

0 件の賞賛
返信
7 返答(返信)

4,675件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @SONGTAOSI,

Have you scoped the bus? Can you show the oscillograms?

What is the LPSPI functional clock and CCR, TCR configuration?

Have you tried increasing the SCKPCS, PCSSCK or DBT parameters?

 

Regadrs,

Daniel

0 件の賞賛
返信

4,665件の閲覧回数
SONGTAOSI
Contributor I

Hi,

Thank fou your reply.

my bus clock is 48MHz, and Function clock is 8M.

LPSPI0_CCR 

SONGTAOSI_0-1678755760114.png

LPSPI1_TCR

SONGTAOSI_1-1678755823838.png

Are there any other conditions required to configure AUTOPCS?

Thanks!

 

0 件の賞賛
返信

4,656件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Thanks @SONGTAOSI, this seems to be correct.

Did you configure the polarity of the selected PCS as described here:

danielmartynek_0-1678796899588.png

 

Regards,

Daniel

0 件の賞賛
返信

4,596件の閲覧回数
SONGTAOSI
Contributor I

Hi,

I  configure the polarity of  PCS0 = 1,selected PTD3 as PCS0,but i configure  PTD3  as GPIO .

SONGTAOSI_0-1680081702246.png

SONGTAOSI_1-1680081786534.png

 

 

タグ(1)
0 件の賞賛
返信

4,592件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @SONGTAOSI,

Does it mean it works now?

 

 

0 件の賞賛
返信

4,589件の閲覧回数
SONGTAOSI
Contributor I

Hi,

Sorry,It still can't work now. Could you please provide a Demo about LPSPI AUTOPCS?Thank you very much!

0 件の賞賛
返信

4,483件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @SONGTAOSI,

I'm sorry for the delay.

Please find the test project attached (S32DS 3.4, SDK RTM 4.0.3)

The slave receives 4 8bit frames in the AUTOPCS mode (1MHz).

danielmartynek_0-1681478844969.png

 

Regards,

Daniel

0 件の賞賛
返信