S32K144 cannot be flashed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 cannot be flashed

2,458 Views
AparnaSridharan
Contributor II

Hi, 

In our customized board we are using S32K144 microcontroller.  While flashing our code for debugging into S32K144 microcontroller using PE micro multilink universal programmer it continuously shows that it is not able to connect with the target processor. 

What are things we have to check so that I can flash the code to microcontroller.

AparnaSridharan_0-1650432793582.pngAparnaSridharan_0-1650432793582.png

 

0 Kudos
Reply
3 Replies

2,447 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi AparnaSridharan,

Please check the "4 Debug and programing interface" of AN5426: Hardware Design Guidelines for S32K1xx – Application Note

And no Power pin should be left unconnected. VDDx and VDDA/VREFH must be shorted together externally to a common reference on PCB.

4 Debug and programing interface.png4 Debug and programing interface.png

 

PORT F or PORT G did you connect to S32K144?( Multilink Universal/Universal FX Tech Summary)

Multilink Universal and Multilink Universal FX Pinouts - Ports A-H.pngMultilink Universal and Multilink Universal FX Pinouts - Ports A-H.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,440 Views
AparnaSridharan
Contributor II

Hi, 

We have connected PORT G with the S32k144 microcontroller. Also all the power pins are connected. 

0 Kudos
Reply

2,429 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Can you halt the MCU by P&E Recovery Utility? refer: Can't use PEmicro debugger with S32K118EVB2-Q048

0 Kudos
Reply