S32K144 ADC sample code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 ADC sample code

9,080件の閲覧回数
SivaB
Contributor III

Hello NXP,

Required tested sample code for 12-bit adc for non autosar application.

SDK version SW32K1_RTD_4_4_1_0_1_D2202.

 

 

0 件の賞賛
返信
4 返答(返信)

9,048件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

The sample codes that are available are as follows:

nxf86756_0-1693332513254.png

Hope it helps you.

Have a nice day!

0 件の賞賛
返信

9,028件の閲覧回数
SivaB
Contributor III

Hi.

I'm using SDK version SW32K1_RTD_4_4_1_0_1_D2202, please share the example code which support tool chain version of 9.3.

S32K1 RTD 1.0.1 available sample code does not have preconfigured ADC setting from CT for non autosar application.

Please refer the attached image and adc pal is not available on S32K1 RTD 1.0.1

 

 

0 件の賞賛
返信

9,014件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

I recommend you to work with S32 Design Studio for S32 Platform v.3.4 and follow the Getting Started below:

Getting Started with the S32K14W-Q064 Evaluation Board

0 件の賞賛
返信

8,985件の閲覧回数
SivaB
Contributor III

Already i have installed all the latest packages, could you share the PDB configuration details for sample code of Adc_Pdb_Ip_example_S32K144.

0 件の賞賛
返信