您好恩智浦团队,
我们团队在使用MCAL之CAN模块时无法发送报文的问题,MCAL版本是S32K1XX_MCAL4_2_RTM_1_0_6评估版,使用EB配置CAN模块的工程如附件文件夹下的MCAL422_EB_project,编译环境使用的是S32 Design Studio for S32 Platform 3.4,主工程如附件文件夹下的MCAL422_S32DS_project。不知是否可以检查我的项目哪里配置或使用不当导致CAN报文发送失败,非常感谢您的支持!
您好,恩智浦团队,
您给我提供的这个链接里面的RTD2.0的安装不知道什么原因一直安装不进S32DS的环境里面,当我将安装文件SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_D2308_DS_Updatesite.zip通过S32 Design Studio for S32 Platform 3.4里面的Install New Software安装时,进度条一直在64%,已经安装两天了,还没有安装完,是否可以提供正确的安装文件和安装步骤,使得S32DS可以正常使用RTD呢?
https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-gener...
The site includes some S32K1xx demo examples based on S32K1 RTD1.0.1 Hot Fix 01.
https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1633067
Thanks!
BR,
Shuang