S32K144搭载S32K1XX_MCAL4_2_RTM_1_0_6以及S32DS编译软件使用CAN模块无法发送报文

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144搭载S32K1XX_MCAL4_2_RTM_1_0_6以及S32DS编译软件使用CAN模块无法发送报文

2,498件の閲覧回数
XIA1414
Contributor II

您好恩智浦团队,

我们团队在使用MCAL之CAN模块时无法发送报文的问题,MCAL版本是S32K1XX_MCAL4_2_RTM_1_0_6评估版,使用EB配置CAN模块的工程如附件文件夹下的MCAL422_EB_project,编译环境使用的是S32 Design Studio for S32 Platform 3.4,主工程如附件文件夹下的MCAL422_S32DS_project。不知是否可以检查我的项目哪里配置或使用不当导致CAN报文发送失败,非常感谢您的支持!

 

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,477件の閲覧回数
Shuang
NXP Employee
NXP Employee

 

Hi,

S32K1XX_MCAL4_2_RTM_1_0_6 is not free to customer. 

I recommend you use S32K1xx RTD2.0 which is based on AUTOSAR 4.4 & R21-11. S32K1xx RTD2.0 is free to all customers.

Below is the download site.

0 件の賞賛
返信

2,428件の閲覧回数
XIA1414
Contributor II

您好,恩智浦团队,

      您给我提供的这个链接里面的RTD2.0的安装不知道什么原因一直安装不进S32DS的环境里面,当我将安装文件SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_D2308_DS_Updatesite.zip通过S32 Design Studio for S32 Platform 3.4里面的Install New Software安装时,进度条一直在64%,已经安装两天了,还没有安装完,是否可以提供正确的安装文件和安装步骤,使得S32DS可以正常使用RTD呢?

XIA1414_0-1694501097256.png

 

0 件の賞賛
返信